CMP#.MODEN

Description

CMP#.MODEN turns the modulo function for the compare channel on or off.

Examples

Usage

0: Turn modulo off (default)

1: Turn modulo on

Code

The following commands turn modulo on for channel 1 and off for channel 2.

--> CMP1.MODEN 1
--> CMP2.MODEN 0

Context

For more information please refer to Compare.

Versions

Action Version Notes
Implemented 02-06-00-000  

General Information

Type

Read/Write

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

See Also

CMP#.MODVAL1, CMP#.MODVAL2
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
CMP1.MODEN

4500h

02h

Unsigned8

-

-

Read/Write

No

CMP2.MODEN

4501h

02h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

CMP1.MODEN

31520

7B20

Unsigned8

Read/Write

-

CMP2.MODEN

31521

7B21

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

CMP1.MODEN

31520

Unsigned8

Read/Write

-

CMP2.MODEN

31521

Unsigned8

Read/Write

-